Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. StruxureWare for Data Centers is actively supported at its own standalone community - https://help.se-dmaas.com/
Hi all,
Can anyone help to set up a redundancy for Struxureware Data Centre Expert VM server ?
Thanks
Hi,
We don't officially support DCE in a disaster recovery scenario.
The only way to achieve redundancy with DCE is to have both servers monitor the same devices and configure them identically. There is no way to sync these servers as they operate independently of each other. If one DCE goes down, the other DCE will still be getting device data. If you make any changes to one DCE, it has to be made manually on the other. I would recommend configuring one DCE, and once that operates to your satisfaction, create a full backup and restore the backup on to a clean DCE.
There is a "Redundant Management Program" offer for licensing the second server in this type of configuration. Details on this are found on the below document.
http://www.apcmedia.com/salestools/RMCR-949E5L/RMCR-949E5L_R0_EN.pdf
Regards,
B
Choose a location
discussion :