Hi All,
So I have a client who bought some 120v-30a IP PDUs (Raritan) but has no where to plug them in.
The current setup:
Two SmartUPS 5000 208v with two step down transformers with a bank of like 12 15 amp standard NEMA15 plugs each.
Can those step downs be outfitted with maybe 6 std NEMA 15s and one+ NEMA L5-30r ? Like are those plug banks modular on the transformer?
Thanks,
Jeff
Choose a location
discussion :