Loading ...

Transfer time specifications of the Symmetra MW | Data Center & Facility 3 Phase UPS

Home » Spaces » Data Center & Facility 3 Phase UPS » discussion » General » Transfer time specifications of the Symmetra MW

Transfer time specifications of the Symmetra MW

Discussion in Data Center & Facility 3 Phase UPS started by Steve , 21 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Transfer time specifications of the Symmetra MW

Subscribe to RSS
  • smclaughlin

    Hello,

    We are looking for the transfer time specifications of the Symmetra MW.

    We need to know the transfer times (in ms) for both the internal bypass and external bypass units for the following actions:

    Bypass to battery/inverter
    Battery/inverter to Bypass

    Some UPS maintenance was being done and when the unit was switched from bypass to normal operation some equipment connected to the UPS lost power.

    We are trying to determine if the time it takes the Symmetra MW to switch between bypass and inverter/battery is less / more than the time our equipment power supplies stay energized once there is a loss of power.

    Thanks,

    Steve


Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7330.14790