Loading ...
Home » Spaces » Data Center & Facility 3 Phase UPS » discussion » General » Battery Temperature Exceeded upper limit

Battery Temperature Exceeded upper limit

Discussion in Data Center & Facility 3 Phase UPS started by Kelum , 12/6/2010 8:24 AM
Login to follow, share, and participate in this space.
Not a member?Join now
  • BATAYA
    Kelum
    Novice Novice
    Kelum 12/6/2010 8:24 AM

    Status:
    UPS: SUVTP15KH-P
    Fault: "*Battery Temperature Exceeded upper limit*"
    Load hovers around *73%-80%*.
    Fault LED lit.

    What does this message mean ? Does this indicate a battery weakness/failure or sensor issue ? The UPS is a newly commissioned unit.

  • ipicKedawinna
    Angela
    =S= Representative
    Angela 12/6/2010 4:55 PM (in response to Kelum)

    it means one of the batteries in the unit may be above its normal operating temperature. are you able to touch the front of the batteries to see if any one string is warmer than the other?

    i am not that familiar with this unit but it seems like a hot battery issue. if it was newly commissioned, it should certainly be covered under the warranty if it turns out to be a faulty battery.

    i would recommend checking the batteries if you can and then you'll probably have to contact support in your region to see if you can have them help you (via phone or service visit)

  • shahzad.engr123
    Muhammad
    Apprentice Apprentice
    Muhammad 10/24/2018 8:40 AM (in response to Angela)

    Hi Angela...

    I am facing Batt Temperature Exceeded Upper Limit, Sometime UPS show system failure by Surveillance error after restart it become normal and again Batt Temp error show.   While i have checked all batt temp is normal i have connected batteries one by one row but issue is still exist. Is there any temp sensor in power module??

    Muhammad Shahzad
  • Page 1 of 1 (3 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692