Loading ...

General | Data Center & Facility 3 Phase UPS

Login to follow, share, and participate in this space.
Not a member?Join now

General

This is a forum for general discussions.

Start Discussion

Error 1-1-5 for Galaxy 4000. 40kVA

by Jesus 2/22/2016 3:45 PM   ·   Last post: Bill 2/22/2016 3:45 PM

Fault CS AC BP

by Jesus 5/12/2016 5:29 PM   ·   Last post: Jesus 5/12/2016 5:29 PM

PX40 IM error

by terrence 3/24/2017 4:17 PM   ·   Last post: Bill 3/24/2017 4:17 PM

fault decoder

by Chandra 10/22/2016 6:20 PM   ·   Last post: schmer 10/22/2016 6:20 PM

What's the best solution ?

by Mohammad 5/31/2016 3:21 PM   ·   Last post: Bill 5/31/2016 3:21 PM

APC Galaxy MGE 300 won't start

by Aqeel 6/16/2016 10:30 PM   ·   Last post: Aqeel 6/16/2016 10:30 PM

Galaxy 5000 80 kVA // Redundant

by Edi 12/17/2016 6:28 PM   ·   Last post: Mojtaba 12/17/2016 6:28 PM

PDU 40kW 208V Display

by Billy 6/29/2015 5:48 PM   ·   Last post: Billy 6/29/2015 5:48 PM

PX SYPM10KF controller question

by Ken 7/15/2015 4:26 PM   ·   Last post: Angela 7/15/2015 4:26 PM

APC smart 30kVA UPS issue

by chuluunbaatar 4/29/2015 1:52 PM   ·   Last post: Angela 4/29/2015 1:52 PM

Data Center & Facility 3 Phase UPS

Space Overview

APC's Data Center & Facility 3 phase power offerings are world class, redundant, scalable, power protection systems designed to cost effectively provide high levels of availability. Typically made up of dedicated and redundant modules--power, intelligence, battery and bypass, all engineered into a design that is easily and efficiently serviceable, this architecture can scale power and runtime as demand grows or as higher levels of availability are required.

Space Administrators

Leave Space :

Are you sure you want to leave this space?

Join this space:

Join this space?

Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

The name that will appear in the space navigation.
The url can point to an internal or external web page.
Choose your language:  
powered by Communifire
Version 6.0.7119.9640