I’m running stand-along system Windows 10 Pro x64, connected to the APC SMT-1500 UPS via USB port. PowerChute Business Edition (v.9.2 build 604) Agent, Server and Console are installed. When I click on the link “Click here” (in the Console window) to proceed to the Outlet Setup screen, it always uses the Microsoft Edge browser. My browser is Firefox by default. I could use the Firefox browser to configure UPS Outlet Groups in Windows 7 Pro x64.
What should I do to make the BCBE v.9.2 console to use the Firefox browser in Win 10 Pro?
System Info:
Windows 10 Pro x64 v20H2
PowerChute Business Edition v.9.2 build 604
Smart UPS SMT1500
Hi,
Launch Firefox, and in the address bar, enter https://localhost:6547 The PowerChute web interface will launch. To save time for future logins, you should bookmark the page.
Choose a location
discussion :