Loading ...

APC Inrow ACRD600P Leak Rope problem | Racks, Rack Accessories, & Cooling

Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » APC Inrow ACRD600P Leak Rope problem

APC Inrow ACRD600P Leak Rope problem

Discussion in Racks, Rack Accessories, & Cooling started by Gabor , 5/16/2019 9:21 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

APC Inrow ACRD600P Leak Rope problem

Subscribe to RSS
  • nova

    Good evening, 

    The Inrow ACRD600P has the function to connect external leak rope to the system. We have connected the leak rope sensor AP9326. But we can’t find in the settings where we can enable this function. We have checked the tuner, and the screen settings and nothing is there, where we can turn on the leak detection function.

    What can be the problem? What is the proper way to connect the leak detector cabel?

  • L2SupportServices-Cooling

    Hello.

    The only option you need to set up for the leak rope is if you want the unit to go to idle on leak detect or if you just want an alarm. This is found under Configuration -> Unit -> Cooling. Select Idle on leak detect. If this is set to Yes the unit will go to idle if the detector see a water leak and generate an alarm. If it is set to no then it will just generate an alarm. This is the only thing you need to set up on the leak detector.

    Thank you

  • nova

    Hi,

    Thanks for your reply.

    Yes, we have this option.

    The question is that why isn’t working the leak rope?

    We have connected it to the leak detection port, we used the right leak rope. There is no option to turn this future on in the tuner software or through the display.

    We have tested the leak rope function and this function is not functional. We have put the leak rope in a bottle of water for 5 minutes and nothing is happening. The controller doesn’t send alarm that there is a leak detection. I have attached two pictures, you can see which firmware version has the ACRD600P inrow unit, the other picture is from the tuner software (no option to turn on the leak rope as you mentioned)

    Is there maybe a newer firmware, which can solve this problem?

  • L2SupportServices-Cooling

    Hello.

    The Idle on leak detect is the option in tuner for this. There is nothing else that needs to be set up in the configuration for the leak sensor. As it is not alarming this would mean the board is not seeing the sensor. We either have a loose connection or a bad leak sensor. Try taking off the leak sensor and jump out the two wires on the molex plug that the sensor plugs into. Leave the jumper on for a minute. If the alarm shows up then it is a bad leak sensor. If it does not then please call into your local tech support and they can help you look for a loose connection or the unit may need a new motherboard set.

    Thank you

Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821