Loading ...

Can acrd500 rack cooling provide power consumption via SNMP | Racks, Rack Accessories, & Cooling

Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » Can acrd500 rack cooling provide power consumption via SNMP
Racks, Rack Accessories, & Cooling

Leave Space :

Are you sure you want to leave this space?

Join this space:

Join this space?

Add a new tab

Add a hyperlink to the space navigation. You can link to internal or external web pages. Enter the Tab name and Tab URL. Upload or choose an icon. Then click Save.

The name that will appear in the space navigation.
The url can point to an internal or external web page.
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Can acrd500 rack cooling provide power consumption via SNMP

Subscribe to RSS
  • timlegge

    Hi

    I am attempting to get a accurate data possible on power ussage in my data center.  Is it possible to obtain power consumption form an acrd500 via snmp?

    Tim

  • L2SupportServices-Cooling

    Hello Timothy.

    There is no value for the overall power draw on the cooling units. There is a value for the compressor drive. The compressor is the main power draw on these units with the fans and condensate pump the other motors in the system. The condensate pump is RATED 240V, 4 AMP, 1/10HP. The fan motor is a Max of 900 watts at 240 for the RD500. They are variable speed fans so the power consumption will vary with the speed of the fans. Hopefully this helps.

    Thank you

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 6.0.7079.4286