Loading ...
Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » High Discharge: Warning - Fix?

High Discharge: Warning - Fix?

Discussion in Racks, Rack Accessories, & Cooling started by Tahmidur , 1/21/2019 5:53 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • Tom_Is_a_Door
    Tahmidur
    New Member New Member
    Tahmidur 1/21/2019 5:53 PM

    I have tried clearing the event log and the alarm log for it to reset and start working again. However, same error keeps popping up. 'High Discharge: Warning'. 

  • L2SupportServices-Cooling
    L2SupportServices-Cooling
    =S= Representative
    L2SupportServices-Cooling 1/22/2019 1:59 PM (in response to Tahmidur)

    Hello Tahmidur.

    Do you have the model number of the unit that this is happening on? Does the compressor ever start on the unit or does it go right to high discharge?

    Thank you

  • Tom_Is_a_Door
    Tahmidur
    New Member New Member
    Tahmidur 1/22/2019 10:25 PM (in response to L2SupportServices-Cooling)

    It turns on, spits out some cool air before start beeping and having a critical light on (red). I think the model is ACRD100

  • L2SupportServices-Cooling
    L2SupportServices-Cooling
    =S= Representative
    L2SupportServices-Cooling 1/23/2019 1:51 PM (in response to Tahmidur)

    Hello. It sounds like there is an issue at the condenser. Make sure that the breaker for the condenser it has not tripped and check if the fan on the condenser start spinning when the unit inside comes on. If the fan is not coming on then an HVAC tech will be needed to check the controls and the motor on the condenser.

    Thank you

  • Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692