Loading ...
Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » Password Reset for Master Switch 9210

Password Reset for Master Switch 9210

Discussion in Racks, Rack Accessories, & Cooling started by Kent , 11/29/2018 5:17 PM
Login to follow, share, and participate in this space.
Not a member?Join now
  • kw1531
    Kent
    Novice Novice
    Kent 11/29/2018 5:17 PM

    Can I still get password reset for an old APC 9210? If so, what info is needed?

  • B-DoubleE
    Matt
    =S= Representative
    Matt 11/29/2018 5:40 PM (in response to Kent)

    Hi Kent,

    In order to reset the password, we would need the serial number of the AP9606 network card installed in the AP9210. With the serial number I can generate a backdoor password you can use with the default username that would allow you to login, and then change the password to what you want.

  • kw1531
    Kent
    Novice Novice
    Kent 11/29/2018 6:53 PM (in response to Matt)

    OK.

    I have three AP9210 units. They are older units with the Ethernet built-in. There is no network card. I have the IP addresses and am able to get to the login prompts via web browser. Here are the serial numbers:

    WA9818878062

    WA9820035326

    WA9913004664

    Thanks in advance!

  • B-DoubleE
    Matt
    =S= Representative
    Matt 11/29/2018 6:57 PM (in response to Kent)

    Hi Kent,

    Backdoor passwords are as follows:

    WA9818878062: 99;4;8^IBB<D

    WA9820035326: 15877<^IBB=<

    WA9913004664: 127:;:^IBC<?

    You'll need to use lowercase "apc" as the username, and attempt to login through either local serial or telnet (it won't work over the web). 

  • kw1531
    Kent
    Novice Novice
    Kent 11/29/2018 7:31 PM (in response to Matt)

    Is it possible that telnet is disabled on the units?

  • B-DoubleE
    Matt
    =S= Representative
    Matt 11/30/2018 3:00 PM (in response to Kent)

    It's possible to disable telnet on the card, so if it's not connecting that's one possible cause (especially if you can pull up the login web page). If telnet is disabled on the card, then unfortunately the only way to reset the password would be locally with the serial cable.

  • kw1531
    Kent
    Novice Novice
    Kent 11/30/2018 3:02 PM (in response to Matt)

    That's what I figured. Is the serial cable just a null modem cable or something else?

  • kw1531
    Kent
    Novice Novice
    Kent 12/21/2018 1:50 PM (in response to Matt)

    Where can I buy the serial cable needed to do this? Or find the correct pinout?

    Kent

  • wpasquil
    Bill
    =S= Representative
    Bill 12/21/2018 3:30 PM (in response to Kent)

    Hi,

    The cable is null modem part number 940-0103. 

  • kw1531
    Kent
    Novice Novice
    Kent 1/11/2019 3:23 PM (in response to Matt)

    Ugh! I drove up to Atlanta, from Orlando to set these up. I got the needed cable and that works - at 19,200, 8, 1, none. But none of these passwords work. I used apc as username (with and without quotes). No joy. I brought the third unit (WA9913004664) and the cable home. Hoping we can get working passwords so I can get these units working.

  • kw1531
    Kent
    Novice Novice
    Kent 1/17/2019 7:24 PM (in response to Bill)

    I got the cable. It works. But none of the logins work.

  • wpasquil
    Bill
    =S= Representative
    Bill 1/17/2019 7:59 PM (in response to Kent)

    HI,

    I re-ran the tool to create the passwords and the ones Matt had provided in November are correct based on the serial number.

    Did you use 2400 baud rate? 

    BTW: As I have entered in other threads support for these units ended a long time ago. 

  • kw1531
    Kent
    Novice Novice
    Kent 1/27/2019 2:19 PM (in response to Bill)

    No. The only speed I can even get to a login prompt with is 19,200. I really don't need much in the way of support. Just working back door passwords. Thanks.

  • Page 1 of 1 (13 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692