Loading ...

Password Reset for Master Switch 9210 | Racks, Rack Accessories, & Cooling

Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » Password Reset for Master Switch 9210

Password Reset for Master Switch 9210

Discussion in Racks, Rack Accessories, & Cooling started by Kent , 11/29/2018 5:17 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Password Reset for Master Switch 9210

Subscribe to RSS
  • kw1531

    Can I still get password reset for an old APC 9210? If so, what info is needed?

  • B-DoubleE

    Hi Kent,

    In order to reset the password, we would need the serial number of the AP9606 network card installed in the AP9210. With the serial number I can generate a backdoor password you can use with the default username that would allow you to login, and then change the password to what you want.

  • kw1531

    OK.

    I have three AP9210 units. They are older units with the Ethernet built-in. There is no network card. I have the IP addresses and am able to get to the login prompts via web browser. Here are the serial numbers:

    WA9818878062

    WA9820035326

    WA9913004664

    Thanks in advance!

  • B-DoubleE

    Hi Kent,

    Backdoor passwords are as follows:

    WA9818878062: 99;4;8^IBB<D

    WA9820035326: 15877<^IBB=<

    WA9913004664: 127:;:^IBC<?

    You'll need to use lowercase "apc" as the username, and attempt to login through either local serial or telnet (it won't work over the web). 

  • kw1531

    Is it possible that telnet is disabled on the units?

  • B-DoubleE

    It's possible to disable telnet on the card, so if it's not connecting that's one possible cause (especially if you can pull up the login web page). If telnet is disabled on the card, then unfortunately the only way to reset the password would be locally with the serial cable.

  • kw1531

    That's what I figured. Is the serial cable just a null modem cable or something else?

  • kw1531

    Where can I buy the serial cable needed to do this? Or find the correct pinout?

    Kent

  • wpasquil

    Hi,

    The cable is null modem part number 940-0103. 

  • kw1531

    Ugh! I drove up to Atlanta, from Orlando to set these up. I got the needed cable and that works - at 19,200, 8, 1, none. But none of these passwords work. I used apc as username (with and without quotes). No joy. I brought the third unit (WA9913004664) and the cable home. Hoping we can get working passwords so I can get these units working.

  • kw1531

    I got the cable. It works. But none of the logins work.

  • wpasquil

    HI,

    I re-ran the tool to create the passwords and the ones Matt had provided in November are correct based on the serial number.

    Did you use 2400 baud rate? 

    BTW: As I have entered in other threads support for these units ended a long time ago. 

  • kw1531

    No. The only speed I can even get to a login prompt with is 19,200. I really don't need much in the way of support. Just working back door passwords. Thanks.

  • kirillmalkin

    Hi Kent, could you please provide a backdoor password for serial WA9943004465? Thank you in advance!

  • kirillmalkin

    Sorry I should have asked Matt, not Kent - my apologies!

  • B-DoubleE

    Hi Kirill,

    The backdoor password for serial WA9943004465 is 1278;;^IBC??

    You'll need to use lowercase "apc" as the username, and attempt to login through either local serial or telnet (it won't work over the web). 

  • kirillmalkin

    Thank you Matt for a quick response, this password worked like a charm!

Page 1 of 1 (17 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821