Loading ...

| Racks, Rack Accessories, & Cooling

Home » Spaces » Racks, Rack Accessories, & Cooling » discussion » General » Model identification 0G-9354-01

Model identification 0G-9354-01

Discussion in Racks, Rack Accessories, & Cooling started by Michele , 1/16/2014 8:06 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Model identification 0G-9354-01

Subscribe to RSS
  • micrenda

    Hello,

    Can someone help me to identify the model of this unit? (see attached screenshot)

    It seems to be the model 0G-9354-01 but in the support section of apc.com site seems it does not exists.

    Does somebody know if there are firmware updates available?

    Thank you in advance

    Michele

    Attachments
  • ipicKedawinna
    This discussion is marked as answered

    This is the model number of a "brain" for an ISX PDU. I don't know what particular model it will be to be honest.

    Yes, there is a firmware upgrade available for the XRDP app - AOS 3.7.5, XRDP 3.7.2. The download SKU is SFPDUM372.

    You can find it @ http://www.apc.com/tools/download/index.cfm under Firmware Upgrades - Modular Power Distribution. Or, since you're using ISX Central, I believe it should show in the upgrade catalog that device offers as this firmware was released, March, 2013.

  • micrenda

    Thank you very much Angela for your support.

    Have a nice day

    Michele

  • Benji

    I am also looking for the current firmware release, could you help me out?

    One of our Symmetra units has 3.7.5 while the other one has 3.7.8, in the download section I can only find 3.7.2 in Modular Power Distribution.

    Also is there some information when the new 0G-9354A (based on NMC2) was released?
    One of the Symmetras is kind of new, but we received it feels like it was shipped with an ancient card...

  • ipicKedawinna

    Hi Benjamin - I can shed a little light on this.

    From what you're saying, you are interested in Symmetra firmware right, not modular PDU (with 0G-9354-01)?

    If so, 0G-9354 latest rev I see is AOS 3.9.0 with px2 app v3.7.7. Here is a link. ftp://restrict:Kop$74!@ftp.apcc.com/restricted/hardware/nmcard/firmware/px2/377/apc_hw03_aos390_px2377.exe 

    Now, 0G-9354A is our Network Management Card 2 brain for Symmetra PX (100, 160, etc) models. It started shipping in supported models units manufactured in 2017. (You can check your UPS's serial number - refer to the first six characters. It should be something like PD1703. 17 refers to the year in my example. If yours says 16, then it was manufactured last year and thus probably came with 0G-9354.)

    0G-9354A replaces 0G-9354 (Network Management Card 1) as you've found. You can apply for an upgrade to this second generation card/brain through your local support team, especially if you just received your UPS unit.

    If you do proceed, let me know if you run into any troubles trying to get 0G-9354A for your new UPSs..

  • tbegush

    Angela.

    My company just bought a Symmetra PX100   Unforunately, we don't have the cable to program the NMC that came with it.   We have a 0G-9354 and in your earlier post you mentioned that it should be a 0g-9354A.    How do I go about getting a replacement? 

  • ipicKedawinna

    Hi Thomas,

    The programming of the IP address for the 0G-9354 can be done through the UPS's powerview display actually if that is all you're looking to do. Cable is not needed specifically for that.

    0G-9354 is fine to use. Unless you need an second generation NMC for any specific reason or special feature, you can continue along with 0G-9354. If you do determine you need a replacement, you should be able to just contact technical support and ask about getting a 0G-9354A. They'll need your UPS serial number to start with.

  • tbegush

    I am impressed with the speed of your reply!   Thank you.   That will give us what we need for the time being!   

  • ipicKedawinna

    You're welcome! (Sorry, this reply was slow with traveling and craziness! winklaughing) .. Happy Thanksgiving!

  • tbegush

    One more question!  :)   

    How do we go about updating the firmware?   

    Hardware Factory

    Model Number: 0G-9354
    Serial Number: QD1702111671
    Hardware Revision: 0C
    Manufacture Date: 01/13/2017
    MAC Address: 00 C0 B7 DB 40 51
    Management Uptime: 0 Days 1 Hour 2 Minutes

    Application Module
    Name: px2
    Version: v3.7.7
    Date: 06/03/2014
    Time: 20:24:48

    APC OS (AOS)
    Name: aos
    Version: v3.7.8
    Date: 06/03/2014
    Time: 18:02:25

  • ipicKedawinna
    This discussion is marked as answered

    Hi again.

    Download this firmware file: ftp://restrict:Kop$74!@ftp.apcc.com/restricted/hardware/nmcard/firmware/px2/377/apc_hw03_aos390_px2377.exe 

    Launch the .exe which is pretty straight forward but specifically, you can review any of the NMC1 firmware upgrade options here http://www.apc.com/us/en/faqs/FA156047 

    It is OK to do this while the UPS is on and operating.

    You'll ultimately only have an update to the AOS component which brings TLS 1.0 and some other little fixes. Your application file will be the same (but still needs to be upgraded as part of the process).

  • tbegush

    Once again, you are the best.   :) 

  • tbegush

    Angela, 

    It appears the NMC that we have 0G-9354 model NMC, which only supports an older firmware that our systems can't support.   Can you please provide a point of contact for me to upgrade our NMC to the -A model? 

  • asbest

    Hello!

    Our company has Symmetra PX 160 with 0g-9354A.
    the web displays the message "Local Management-To-UPS Communication Lost". After replacing the monitoring card,  problem remains.

    Network Management Card AOS v6.5.0

    Will the firmware update help?

  • wpasquil

    Hi,

    What firmware is on the card now? You will find that information under the About tab.

  • asbest

  • wpasquil

    Hi,

    I checked with the 3 Phase support team in North America and they recommend you call local support for assistance. Local support information will be found at this link.

    https://www.apc.com/us/en/support/contact-us/index.jsp

     

Page 1 of 1 (17 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049