Loading ...

AP9630 Firmware Upgrade on SRT3KXLI? | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » AP9630 Firmware Upgrade on SRT3KXLI?

AP9630 Firmware Upgrade on SRT3KXLI?

Discussion in Smart-UPS & Symmetra LX / RM started by TimothyFinn TimothyFinn , 5/8/2020 1:24 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

AP9630 Firmware Upgrade on SRT3KXLI?

Subscribe to RSS
  • TimothyFinn

    My SRT3KXLI ups does recognize my AP9630 and i have been having issues upgrading my NMC2 on SRT3KXLI who AOS version is 6.7.0, the bootmon is 1.0.8 and sumx is 6.7.2. However, using the hyperterminal method of upgrade, i.e using the XMODEM to receive the upgrade bin. files, i upgraded the sumx to version 6.8.2 first inste https://solitaire.onl/ ad of the normal procedure of upgrading the bootmon, then the aos, the the app. sumx. 

    Moreover, i have been trying since then to upgrade the bootmon and the aos versions buthttps://9apps.ooo/  it is not going through, and i have sine reset the nmc several times if it can be done from start but to no avail. 

    Please, kindly help give solutions as the only means of NMC2 upgrade is through the use of hyperterminal (teraterm) i.e XMODEM 

    thanks.

  • wpasquil

    Hi,

    The instruction for upgrading AP9630 firmware are available in Schneider Electric FAQ FA156047

    There is also FAQ FA293874 Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware.

     

  • kahml

    Bill, that second link doesn't go to a document:

  • wpasquil

    Hi,

    I have fixed the link.

Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 7.0.7485.25369