Loading ...

SMX1500RM2U w/External Packs Strange Runtime | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » SMX1500RM2U w/External Packs Strange Runtime

SMX1500RM2U w/External Packs Strange Runtime

Discussion in Smart-UPS & Symmetra LX / RM started by John , 4/18/2020 4:17 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

SMX1500RM2U w/External Packs Strange Runtime

Subscribe to RSS
  • jmiller31

    I have a number of these units but this one in particular is doing something really strange. It has 2 external packs and until yesterday had about an output load of about 38% and it was consistently reporting a run time in the 40-45 minute range. Yesterday I added a server to it which brought the load up to 55%, the runtime immediately went down to the 3 to 6 minute range.  That just doesn't any sense to me even if I had doubled the load the runtime should be around 20 minutes, it's acting like I'm close to 100% load.

    I ran a calibration and after calibration I'm still down in the 3 to 6 minute range. The more I've looked into this even the 40-45 minute range doesn't make sense. According to APC's charts this unit with 2 external packs at half load should get a runtime of 2 hours. Now I realize that's in a perfect world so I wouldn't expect to get 2 hours but it should be off this much. BTW I'm looking at all this data using an NMC2.

    Anyone have any thoughts? A bad UPS?

    Thanks,

     

    John

     

  • older

    Hi John


    I had similar symptoms a year ago - SMT1500RMI2U PCB: 640-3081J-Z-001 Tg = 170 SMT1500RMI.
    Network equipment was connected to it with a load of about 50%. During automatic testing with a period of 14
    days, UPS for some reason undelete the entire load without leaving NMC2 (AP6930) logs - no traces and no replicas
    in the LAN.
    By agreement with the personnel at the remote site, I gave the command through AP6930 to perform a test with the
    transition to the battery and the load was disconnected. If you decide to do the same, then pay attention to
    THIS!
    I have been reading this forum for almost a year and you have now outlined what has been directly or indirectly
    mentioned here more than once.
    In short, I decommissioned the UPS in this series. Moreover, the platform or circuitry is the same for many UPSs
    of this generation.
    The only recommendation has always been Braindead or bring it to the service.
    No one is even trying to explain the true cause or admit a mistake in the circuit.
    Outrageous
    and ashamed!

    Vladimir.

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7485.25369