Loading ...

No 4ft 96VDC Extension Cable Available? | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » No 4ft 96VDC Extension Cable Available?

No 4ft 96VDC Extension Cable Available?

Discussion in Smart-UPS & Symmetra LX / RM started by Seb , 11/11/2019 2:41 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

No 4ft 96VDC Extension Cable Available?

Subscribe to RSS
  • SebJS

    Hi There,

    I'm building a solution with a Smart-UPS SRT 3000VA RM and a Smart-UPS SRT 96V 3kVA RM Battery Pack however due to the design there will be quite a space between the two meaning that the standard cable will likely not be long enough.

    I notice there are a number of 4ft cables available but none for 96VDC, the only available extension I can see is15ft which is far too long.

    Could I use the 4ft APC Smart-UPS X 120V Battery Pack Extension Cable (SMX040) in place of the 15ft Extension Cable for 96VDC External Battery Packs 3000VA UPS (SRT010)?

    Or could someone point me in the direction of an appropriate 4ft cable?

    Any advice is gratefully receive, Thank you.

  • MattK

    Hi Seb

     

    Unfortunately the connectors on the SRT010 and the SMX040 and the sockets on their respective UPS are keyed differently, so they aren't compatible.

    Looking through our product accessory offer, I don't see any other cable apart from the 15ft cable.

    Regards

    Matt

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049