Loading ...

Fan control on SRTL1500RMXLI | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » Fan control on SRTL1500RMXLI

Fan control on SRTL1500RMXLI

Discussion in Smart-UPS & Symmetra LX / RM started by Karol , 9/17/2019 8:00 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Fan control on SRTL1500RMXLI

Subscribe to RSS
  • DrKarol

    Hello all,

    I have just upgraded from a quiet SMX1500RM2U to a loud SRTL1500RMXLI.  I was going after the Lithium-ion battery, but I did not realise that the fan would be always running at full speed on the new SRTL1500RMXLI.  Is there any possibility that APC might develop a firmware for the SRTL1500RMXLI that would allow variable fan speed/control?  I have the UPS installed in my home office with ambient temperatures around 20 degrees Celsius, and with constant full speed fan it is running at a very low internal temperature.  I am sure it could easily run with the fan at much lower RPM during normal operation just as the older SMX1500RM2U.

    Best regards,

    Karol

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049