I have a new (to me) APC.
I have the following warning/error notifications:
Local Management-To-NMC Integrated EM Sensor Communication Lost (Port 1 and 2).
I do not plan to use this feature at all.
How can I shut this off or ignore?
Little new to the device and I'm not finding an area to "ignore" these ports
Hello,
On 8/23/2019 11:08 AM, Cory said: Local Management-To-NMC Integrated EM Sensor Communication Lost (Port 1 and 2). I do not plan to use this feature at all. How can I shut this off or ignore?
Open the NMC web interface and go to Configuration, Notification, Event Action, By Event. Select Communication and click on Environment: Lost the local network management interface-to-integrated Environmental Monitor ({name} at {location}) communication. Then deselect logging, email, trap.
I have done this, but it appears this is a built-in alert?
(see attached)
Choose a location
discussion :