Loading ...

SMT3000C Change Input Connection from 30a to 15a | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » SMT3000C Change Input Connection from 30a to 15a

SMT3000C Change Input Connection from 30a to 15a

Discussion in Smart-UPS & Symmetra LX / RM started by David , 7/19/2019 2:44 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

SMT3000C Change Input Connection from 30a to 15a

Subscribe to RSS
  • Lioninstreet

    The SMT3000C input cable runs a NEMA L5-30P 30a 120v input plug.

    Problem is, I don't happen to have a 30a circuit readily available. But I heard it was possible to change the input connection & cabling from the 10 gauge cable / L5-30 plug to something like a 12-14 gauge cable / 15a NEMA 5-15p plug.

    I'm actually seeing SMT3000 units being sold on eBay with 120v 5-15p power input plugs on them so I have to believe the change over cant be rocket science.

    Would anyone with experience with this know if besides swapping out the cable & plug end, are there any internal switching changes that need to be made so the current draw is limited to the smaller size input circuit??

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049