Loading ...

temperature sensor | Smart-UPS & Symmetra LX / RM

Home » Spaces » Smart-UPS & Symmetra LX / RM » discussion » General » temperature sensor

temperature sensor

Discussion in Smart-UPS & Symmetra LX / RM started by gaconvn , 3/1/2019 3:02 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

temperature sensor

Subscribe to RSS
  • gaconvn1106
    Temperature sensor disconnected
    I have just installed the temperature sensor that comes with the UPS
    The ups model is a Smart-UPS SRT 10000 (SRT10KRMXLT)
    All went well and configured alerts for minimum and maximum value.
    Then a few minutes later I enable SSH access and need to reboot management interface.
    Since then the sensor is not detected.
    SSH is OK but not the temperature sensor.
    The NMC2 is at latest firmware v6.6.4
    What's is the problem ?
    Thanks

  • wpasquil

    Hi,

    What port do you have the sensor connected to and when enabling SSH are you entering a host key? 

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049