Loading ...

Battery disconnected | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Battery disconnected

Battery disconnected

Discussion in Back-UPS & Surge Protectors started by Richard , 19 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Battery disconnected

Subscribe to RSS
  • I have a brand new SMT1500RM1U UPS that i installed in a rack, connected the battery pack in front and plugged in to an AC (119 VAC) source. 

    When the unit powered up and did self test i received an error indicating "Connect battery" with audible alarm and red led flashing.  is there anything that has to be done during initial power up other than this? I have not checked the voltage at the battery as of yet, but the unit was just purchased, shipped to the installation site and plugged in.  I will get the serial number and more details tomorrow, but wanted to check to see if there was something i did not do during the initial power up?

    Thanks

     

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 8.0.7757.16597