Loading ...

Back-UPS 700 shutting down | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Back-UPS 700 shutting down

Back-UPS 700 shutting down

Discussion in Back-UPS & Surge Protectors started by Chris , 15 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Back-UPS 700 shutting down

Subscribe to RSS
  • I have the above model and I have been having a strange problem as of late. The UPS doesn't switch to battery power during a blackout and shuts down immediately as if the battery failed. Sometimes it will stay on for a few seconds making short beeps. However, if I disconnect the USB/Data port cable the UPS seems to be working normally during a blackout. I have a 500W PC & monitor connected to the UPS.

    The unit is about 10 years old and I just bought a new 7.2 Ah battery. Does anyone know what might be the problem? Could it be a faulty battery?

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 8.0.7757.16597