Loading ...

Back-UPS Pro 900 AVR and Error Light Flashing | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Back-UPS Pro 900 AVR and Error Light Flashing

Back-UPS Pro 900 AVR and Error Light Flashing

Discussion in Back-UPS & Surge Protectors started by Nick , 2/11/2021 7:03 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Back-UPS Pro 900 AVR and Error Light Flashing

Subscribe to RSS
  • Hi,

    My Back-UPS Pro 900 UPS is indicating an error which I cannot identify from any manual. The AVR indicator on the LCD is flashing together with the System Fault indicator. The UPS also then beeps 3 times every minute. No fault code is shown on the LCD display. When the AVR indicator is flashing, the indicator for low or high input power does not show.

    When powered on all the systems checks are completed without error. About a minute after system checks are completed the above error starts showing up.

    Input power is fine, and batteries have been replaced recently.

    Any help will be appreciated.

     

  • On 2/11/2021 12:33 PM, Nick said:

    Hi,

    My Back-UPS Pro 900 UPS is indicating an error which I cannot identify from any manual. The AVR indicator on the LCD is flashing together with the System Fault indicator. The UPS also then beeps 3 times every minute. No fault code is shown on the LCD display. When the AVR indicator is flashing, the indicator for low or high input power does not show.

    When powered on all the systems checks are completed without error. About a minute after system checks are completed the above error starts showing up MyLowesLife.

    Input power is fine, and batteries have been replaced recently.

    Any help will be appreciated.

     

    Over temperature On Battery - UPS has exceeded the over temperature threshold. Note: The UPS will beep and the red LED will illuminate till the internal temperature reaches the normal range for 5 minutes before the UPS shuts down.

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 8.0.7842.9669