What are the differences between these two units? Both are 1500va with 10 outlets, approximated sine. What else?
The BN unit seems to be a slightly upgraded model with better surge protection and an ever so slightly improved battery life.
-Gavan
On 12/8/2020 2:00 PM, Gavan said: The BN unit seems to be a slightly upgraded model with better surge protection and an ever so slightly improved battery life. mygroundbiz.com -Gavan
The BN unit seems to be a slightly upgraded model with better surge protection and an ever so slightly improved battery life. mygroundbiz.com
Hmm... Thanks for the information.
Choose a location
discussion :