Loading ...

BX1500G Beeps Twice Every Two Seconds? | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » BX1500G Beeps Twice Every Two Seconds?

BX1500G Beeps Twice Every Two Seconds?

Discussion in Back-UPS & Surge Protectors started by CollinIsmael , 6/11/2020 8:24 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

BX1500G Beeps Twice Every Two Seconds?

Subscribe to RSS
  • CollinIsmael

    My BX1500G beeps twice every two seconds and an empty battery symbol flashes in-sync with the beeps.  I removed the batteries, waited 30 minutes and reinstalled the batteries. This made no difference.  It does this for as long as the unit is plugged into the wall and turned on.  Anyone know what the cause of this is or what a solution might be?

     

  • Mauricio

    Hola.

    Actualmente tengo ese problema.

    De soporte de Mexico me indicaron que se debe llevar a un centro autorizado.

    El problema es que la batería no se detecta.

    Tengo que llevar el UPS

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049