Loading ...

Continuous discharge - recharge cycle | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Continuous discharge - recharge cycle

Continuous discharge - recharge cycle

Discussion in Back-UPS & Surge Protectors started by Alex , 5/7/2020 2:15 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Continuous discharge - recharge cycle

Subscribe to RSS
  • ak47

    I have a APC Back-UPS RS 550 that's been fine for many years. I have replaced the battery a few months back. Lately the UPS seems to be in a continuous discharge recharge cycle. I have the UPS hooked up to a linux server via NUTS and it is recoding this information. I have attached a few charts of the charge cycle that shows the problem.

    I have checked load charts and they show a steady 20% load with minor bumps to around 35%. The voltage charts show 245 -250 volts typically.

    What could be causing the discharge recharge cycle?

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7485.25369