Loading ...

Immediate help: APC Back-UPS 600 switch on button and battery LED constant red | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Immediate help: APC Back-UPS 600 switch on button and battery LED constant red

Immediate help: APC Back-UPS 600 switch on button and battery LED constant red

Discussion in Back-UPS & Surge Protectors started by Little , 4/6/2020 7:12 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Immediate help: APC Back-UPS 600 switch on button and battery LED constant red

Subscribe to RSS
  • Greenblue

    APC Back-UPS 600 switch on button and battery LED are constantly in red. No sound. No power connection. The device is not heating up. 3-4 years since purchase and usage. But the LEDs are working. Does it have possibility to explode? Please help. 

  • lennyburns

    It won't explode. :)

    Especially with no heat.

     

    Just stop using it and pull the battery out.

    See if it will work as a power strip on the unprotected plugs.

    If yes, just replace the batteries.

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7485.25369