Loading ...

Not charging battery Backups pro 1500 | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Not charging battery Backups pro 1500

Not charging battery Backups pro 1500

Discussion in Back-UPS & Surge Protectors started by Aashish , 9/8/2019 8:53 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Not charging battery Backups pro 1500

Subscribe to RSS
  • As13

    Ok so everything was normal i connected the ups to a power source and then bam i hear a voice in the background not from the ups and the general power just goes off, my ups protects the pc i had connected to it but when i restart the ups it doesn't recharge the battery, could anyone help a novice out

     

     

    Thanks

    Attachments
  • wpasquil

    Hi,

    Try resetting the UPS

     1: Disconnect any attached load.

    2: Unplug the UPS from the wall socket.

    3: Disconnect the UPS' internal battery.

    4: Push and hold the "On" button on the UPS for 5 seconds

    5: Reconnect internal battery.

    6: Plug UPS in to known good power source.

    7: Turn UPS on.

    If it still will not charge after the reset that would indicated the charging circuitry took a hit during the power outage and the UPS should be replaced. 

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821