Loading ...

BN1100M2 incorrect load reporting? | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » BN1100M2 incorrect load reporting?

BN1100M2 incorrect load reporting?

Discussion in Back-UPS & Surge Protectors started by Mark , 8/2/2019 12:01 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

BN1100M2 incorrect load reporting?

Subscribe to RSS
  • mc04

    Just got a new Back Ups BN1100m2. With just my monitor and speakers connected to battery, it reports about 21W, dropping to 1W when they're sleeping. But if I unplug the UPS from the wall while the monitor and speakers are on, both continue working normally but the reported load suddenly drops to 3-5W. What's going on here?

  • mc04

    Update: I've read that apparently inaccurately reporting small loads is a shortcoming of these units, but even loaded up to a little more than 300W it still reports about 260W when switched to battery. Is it faulty?

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821