Loading ...

ProtectNet PTEL2 OR PNET1GB ?? | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » ProtectNet PTEL2 OR PNET1GB ??

ProtectNet PTEL2 OR PNET1GB ??

Discussion in Back-UPS & Surge Protectors started by Augusto , 7/11/2019 7:54 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

ProtectNet PTEL2 OR PNET1GB ??

Subscribe to RSS
  • Mrmind

    I have a phone/internet connection FTTC VDLS2 (bandwidth frequency: 17-35 MHz), with a "Technicolor 768600" gateway (router+modem).
    On the wall there's an outlet with 2 phone jacks (RJ-11 ports); a light gray cable comes out of the 1st port, with only 2 wires and the two central pins (n. 2 and 3), which plugs into the gateway VDSL2 port ; from the other port of the outlet a black cable comes out, always with only 2 wires and two central pins (n. 2 and 3), which plugs into the gateway LINE 1 port (IN).
    At the gateway LINE 2 port (OUT) a phone cable connects a fax modem inserted into my PC, a fax machine / printer multifunction to which the telephone and the t.a.m. are connected.
    The gateway PSTN port is empty.
    The gateway Ethernet port 1 is connected, by an Ethernet cable, to my Switch port 1. To the other 7 Switch ports the various network devices are connected: PC, scanner, etc.

    To protect the fax modems, the gateway (router+modem) and the ethernet/switch network from overvoltages, do I have to use the APC ProtectNet for phone lines PTEL2 OR the ProtectNet for Ethernet lines PNET1GB ? Or both of them?
    Where should I mount it/them ?
    Thanks for the tips.

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7330.14790