Loading ...

Best practice for the UPS after the connected PC or device is turned off | Back-UPS & Surge Protectors

Home » Spaces » Back-UPS & Surge Protectors » discussion » General » Best practice for the UPS after the connected PC or device is turned off

Best practice for the UPS after the connected PC or device is turned off

Discussion in Back-UPS & Surge Protectors started by Andrei , 6/10/2019 10:04 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Best practice for the UPS after the connected PC or device is turned off

Subscribe to RSS
  • andreiguird

    Which is the best practice for the UPS after the connected computer is shut down?

    1) Turn off the UPS but let the UPS still plugged to main outlet (keep charging the battery)

    2) Turn off the UPS and also disconnect it from main outlet (the battery would discharge slowly in this state)

    3) Let the UPS keep turned on.

     

    I have tried the 1st one, the UPS will keep getting warm while it's turned off. Would this affect longevity of the components inside?

    For the 3rd one, if I'm not in home and there is blackout, the UPS will turn into battery mode and the battery will keep discharging until it's run out. If it often happens, would this reduce the battery life greatly compared to 2nd method ?

  • wpasquil

    Hi,

    Option one would be the best. The UPS will keep the battery at an optimal charge level and no it will not affect the longevity of the battery or UPS.  

  • Onest1997

    Hello Dear,

    Your forum is so nice i read it carefully all information are good and helpfull.i share your forum and information with my friends and different groups because your forum is so attractive.

  • manu44
    This discussion is marked as answered

    Hi,

    Is it better turn off the switch of the PSU before turn off the UPS?

    And if its better to first turn on the UPS before turn on switch of the PSU?

    Does it matter?

    It´s dificult to me for reach PSU switch and i wanna know if its bad do after shutdown the pc turn off the UPS while the switch of the PSU still on?

    Thank you very much

Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821