Loading ...
Home » Spaces » Back-UPS & Surge Protectors » discussion » General » battery discharging with no power alerts

battery discharging with no power alerts

Discussion in Back-UPS & Surge Protectors started by Chris , 19 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
  • borochris
    Chris
    Novice Novice
    Chris 19 days ago

    Twice in the last 2 weeks the battery has discharged to 50% with accompanying audible alert but there is nothing in the power alert history and another unit next to it has not gone to battery.

    The alert tone was still happening when the battery got to 100%.

    When it finally got back to 100% I did a self-test. This passed but suddenly the battery was at 47%.

  • borochris
    Chris
    Novice Novice
    Chris 12 days ago (in response to Chris)

    This is now regularly (every couple of days) sounding an alert tone with battery showing 100% and no events.

    Anyone else seen anything like this?

  • TomC
    Thomas
    =S= Representative
    Thomas 10 days ago (in response to Chris)

    Hi Chris,

    Can you please provide the model and serial number of this UPS to help us troubleshoot this issue.

    Has the battery in the UPS been replaced previously? If so, when was this replaced?

    Regards,

    Tom

  • borochris
    Chris
    Novice Novice
    Chris 9 days ago (in response to Thomas)

    Model: Back-UPS XS 1400U
    Serial number: 3B1637X21134
    Firmware revision: 926.T2.I
    Software version: PowerChute Personal Edition 3.0.2
    Date of last manual self-test: Never
    Result of last manual self-test: Not Recorded
    RAM: 5.99 GB
    Free disk space: 18078.21 GB

    Despite what it says I did a self-test through the app and have now (took a few days to organise) done a full power off and restart.

    The unit is only 2 1/2 years old so have not replaced the battery.

    Unfortunately the app now says remaining battery charge unknown and battery is currently unknown. This is obviously not satisfactory and very worrying.

  • Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 5.2.6420.11692