Hello,I recently purchased a new UTS10BI for work with a Honda EM4500SX generator whit remote control kit.I have a very good UPS model Smart-UPS 3000 RM X 240 Volt model.I need that when power outages from watt hour meter for a long time the universal transfer switch automatically turns on the generator and do not download all the batteries of the UPS.omegle xenderI have connect the wire 9 IN and 10 IN to my 240 Volt in watt hour meter but the UTS10BI not power on,only i hear a relay close,no leds and no disply switch on.To be able to turn and see the operating uts I have purchased a 240 volt transformer primary 240 Volt and secondary 120 Volts 300 VA and I plugged the cable into the UPS Inlet.Please can you help me, I spent a lot of money, time and no one knows how to help me to connect these devices.I already called two professionals but they do not know the UTS10BI.
Many thanks!
Choose a location
discussion :