Loading ...

the APC UTS 10BI | Universal Transfer Switch

Home » Spaces » Universal Transfer Switch » discussion » General » the APC UTS 10BI

the APC UTS 10BI

Discussion in Universal Transfer Switch started by jurick , 3/4/2020 8:12 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

the APC UTS 10BI

Subscribe to RSS
  • jurick

    I recently purchased the APC UTS 10BI.  My problem is my main panel has three different 240V pole circuits, and each one is different.  One has two 15 A breakers for the extra basement heater (not used much at all).  Another has two 20 A breakers for the extra oven in the kitchen.  The third has two 30 A breakers for the electric drier.  I'm still not sure about what I "want" to use for the 240, but is it safe to use any of the circuits even if the breakers are not 20A?

     

    Thanks in advance!

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7330.14790