Loading ...

| Universal Transfer Switch

Home » Spaces » Universal Transfer Switch » discussion » General » APC UTS6H wired to two Honda EU2000i (one companion model) in parallel 30 amp output

APC UTS6H wired to two Honda EU2000i (one companion model) in parallel 30 amp output

Discussion in Universal Transfer Switch started by Michael , 9/15/2014 6:57 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

APC UTS6H wired to two Honda EU2000i (one companion model) in parallel 30 amp output

Subscribe to RSS
  • cini

    What value should I enter for my genset configuration while setting up the APC UTS6H for Gen Power Rating?   The maximum output is ~4000 watts, but at no more than 30 minutes at any one time.  The running wattage is 3200 watts.  So do I enter 3200 or 4000  watts for the Gen Power Rating?    Tx!

  • ipicKedawinna

    We recommend setting it to 3200 watts to avoid problems for your setup. We sometimes recommend customers choose something between the running wattage and the peak wattage. Also, adaptive load management will kick in to help out.

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7446.33821