Loading ...

[Image attached] Is this type of setup allowed to connect devices to an APC UPS? | General Questions & Suggestions

Home » Spaces » General Questions & Suggestions » discussion » General » [Image attached] Is this type of setup allowed to connect devices to an APC UPS?

[Image attached] Is this type of setup allowed to connect devices to an APC UPS?

Discussion in General Questions & Suggestions started by Michael , 15 days ago
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

[Image attached] Is this type of setup allowed to connect devices to an APC UPS?

Subscribe to RSS
  • mapc

    Hello.

    Can I connect my devices to an APC UPS using an IEC C14 to 4 Way Gang UK Mains Sockets Lead like the attached and the below:

    https://images-na.ssl-images-amazon.com/images/I/71jRheuOJlL._AC_SX679_.jpg

    Of course the load of all my devices will not exceed the total load of the UPS.

    I ask because I was checking this page and I would like to have confirmation before proceeding with the setup I have in mind:

    https://www.se.com/us/en/faqs/FA158852/

    Thank you.

    Attachments
  • APC_Gavan
    This discussion is marked as answered

    Provided the 4 way adapter doesn't have any surge protection and operates as a straight cable then your should be okay.

    -Gavan

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 8.0.7598.8416