Hello.
Can I connect my devices to an APC UPS using an IEC C14 to 4 Way Gang UK Mains Sockets Lead like the attached and the below:
https://images-na.ssl-images-amazon.com/images/I/71jRheuOJlL._AC_SX679_.jpg
Of course the load of all my devices will not exceed the total load of the UPS.
I ask because I was checking this page and I would like to have confirmation before proceeding with the setup I have in mind:
https://www.se.com/us/en/faqs/FA158852/
Thank you.
Provided the 4 way adapter doesn't have any surge protection and operates as a straight cable then your should be okay.
-Gavan
Choose a location
discussion :