Loading ...

regarding connections to ups | General Questions & Suggestions

Home » Spaces » General Questions & Suggestions » discussion » General » regarding connections to ups

regarding connections to ups

Discussion in General Questions & Suggestions started by krovvidi , 8/18/2020 5:30 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

regarding connections to ups

Subscribe to RSS
  • krovvidi17

    I recently bought a Backup ups 600. Can the ups be plugged in  on to the pc, wifi router etc. at all times 

  • wpasquil

    Hi,

    Yes. You should plug the PC and router into a battery/surge outlet. Plugging into the battery/surge outlets will provide battery back up in the event of a power failure. 

  • Tualatin56

    In case of emergency breakdown when utility power is not available from the powerhouse, we may use automatic inverter / UPS and batteries to connect the power without interruption.

    We will show two basic UPS / Inverter with batteries connection to the home distribution board.

    • Auto UPS / Inverter with Two Wires
    • Automatic USP / Inverter Wiring with One Live Wire

    Note: To be in safe mode, use 6 AWG (7/064″ or 16mm2)  to connect the UPS to the main panel board.

     

    myprepaidcenter

Page 1 of 1 (3 items)
Choose your language:  
powered by Communifire
Version 8.0.7607.8929