Loading ...

Control Back-UPS through Network | General Questions & Suggestions

Home » Spaces » General Questions & Suggestions » discussion » General » Control Back-UPS through Network

Control Back-UPS through Network

Discussion in General Questions & Suggestions started by Laurie , 4/30/2020 2:01 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Control Back-UPS through Network

Subscribe to RSS
  • lmstearn

    Hi there,

    Have minimal home config consisting of a NAS and two computers, A & B connected by Ethernet. The Back-UPS RS 900G powers the NAS and computer A. Computer B, some distance away, is powered by another UPS, and uses the Synology DS218+ drives over the Ethernet. The Synology DSM on that machine interfaces nicely with the Back-UPS as shown in this snapshot:

    Question is, are there any APC utilities that can interact with the UPS remotely via the Ethernet as the above does? Or does the entire APC app require installation on computer B?

    Thanks.

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7489.18715