Loading ...

Converting output from 230 to 115 VAC | General Questions & Suggestions

Home » Spaces » General Questions & Suggestions » discussion » General » Converting output from 230 to 115 VAC

Converting output from 230 to 115 VAC

Discussion in General Questions & Suggestions started by peter , 3/25/2020 11:25 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Converting output from 230 to 115 VAC

Subscribe to RSS
  • petec

    I have a SURT1000XLI. Got it from work. It was used on a piece of decommisioned equipment.

    Would like to use at home. Is there a way to easily convert the output to 115? How about the input?

    I am hoping it is as easy as moving a jumper somewhere.

    Also, could I use it for extended periods, if I add enough battery, or are these things designed to run stuff just long enough to power down safely?

    Thanks,

    Pete

  • Brad_C
    On 26/3/2020 7:25 AM, peter said:

    I am hoping it is as easy as moving a jumper somewhere.

    No.

    On 26/3/2020 7:25 AM, peter said:

    Also, could I use it for extended periods, if I add enough battery, or are these things designed to run stuff just long enough to power down safely?

    It's an XL, so yes it is designed for additional battery.

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 7.0.7489.18715