Loading ...

UPS for a little company | General Questions & Suggestions

Home » Spaces » General Questions & Suggestions » discussion » General » UPS for a little company

UPS for a little company

Discussion in General Questions & Suggestions started by White , 3/21/2020 5:17 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

UPS for a little company

Subscribe to RSS
  • WhiteTiger

    I have to buy a UPS and I'm going to a SmartUPS.
    I only have to connect:

    • 1  Dell server
    • 1 or 2 PC
    • 1 or 2 Raspberry
    • 1 switch 24 ports
    • 1 router

    With an instrument I measured the values for about half a day and I detected these:

    • V 219.5
    • Amp 1.31
    • W Between 255 and 261
    • W Max: 330
    • Power Factor between 81 and 89
    • KW / h 1.5

    VMWare ESXi 6.7 is installed on the Dell server with 7 VMs that turn off one after the other within about 15 minutes.

    I then have 5 other PCs, each with its own UPS.
    I would like to install Powerchute to control the shutdown of the main PCs, Raspberry, VMs and ESXi server.
    Possibly I would also like to send a signal to the other PCs so that they can be turned off.

    My budget is modest and I would like to stay under € 1,000; possibly around € 800 at the most.
    Which SmartUPS model do you recommend?

    Thanks in advance for any advice.

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 7.0.7489.18715