Loading ...

Update Firmware and Configuration of Netbotz 250 with a distant Linux | NetBotz - StruxureWare Hardware & Software

Home » Spaces » NetBotz - StruxureWare Hardware & Software » discussion » General » Update Firmware and Configuration of Netbotz 250 with a distant Linux

Update Firmware and Configuration of Netbotz 250 with a distant Linux

Discussion in NetBotz - StruxureWare Hardware & Software started by Raphael , 3/14/2019 3:15 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Announcement 

Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.ecostruxureit.com/questions

Posted in: General

Update Firmware and Configuration of Netbotz 250 with a distant Linux

Subscribe to RSS
  • Hello everyone,

    I am currently working on a system composed of a BOT (automated Linux) piloting the distant Netbotz 250.

    The BOT will have to perform automatically an upgrade of the firmware (bootmon, AOS, Application modules) and the configuration.ini automatically. Of course, these files will have been added on its harddrive previously.

    in addition, the BOT can only use the commands ssh commands (e.g. scp). It has no ftp and cannot use an executable to perform the action.

    I would like to know what is the correct procedure to do, to perform such updates (firmware and configuration). All I have read in the datasheet is about the transfer (scp) of the files on the Netbotz.

    Is that really all the BOT need to do ? What is happening on the Netbotz 250 after the files have been copied via scp?

    Thank you in advance for your answers to my questions.

    Best Regards,

    rf2019

  • Hello,

    NetBotz are actively supported at its own standalone community - https://help.ecostruxureit.com/questions

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 8.0.7757.16597