Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.ecostruxureit.com/questions
So today we observer something very odd. At various times today at multiple sites on our network in different states we are seeing our head units alert that they have been unplugged or malfunctioned. Log into the units and they are fine. Has anyone ever seen this across and entire organization? I have seen various network scans trigger alerts on UPS mgnt. for things like SNMP but this is a first.
Update to when this was first posted. All the devices reply with a ping but fail to connect from either web or Advanced view (4.5.3). At a site where we have on prem staff, a cold reboot resolved this. Problem remains however, what might cause this.
Hi,
NetBotz are actively supported at its own standalone community - https://help.se-dmaas.com
Choose a location
discussion :