Loading ...

Power control using netbotz 550 | NetBotz Hardware & Software

Home » Spaces » NetBotz Hardware & Software » discussion » General » Power control using netbotz 550

Power control using netbotz 550

Discussion in NetBotz Hardware & Software started by Donny , 7/8/2010 4:39 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Announcement 

Note: No new discussion posts are allowed in this area. Historical content is for viewing purposes only. NetBotz are actively supported at its own standalone community - https://help.ecostruxureit.com/questions

Posted in: General

Power control using netbotz 550

Subscribe to RSS
  • TaSpEc

    Yes you can configure the 550 to shutdown outlets on a pdu. This kbase discusses the required cables and firmware http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=9299

    Be aware that with the netbot connected to the pdu via serial, only the netbot will have access to the device, since the serial port takes priority over telnet and web access. Also there is a known issue with multi-bank pdus. Hope this information helps.

  • worshiprocker

    Thanks for the reply that is exactly the information I needed.

  • Bloke

    This knowledge base article no longer exists but I think I need this exact information. Anyone able to help me?

  • TaSpEc

    This kbase should be back up in the next 24-48 hours, I would recommend checking back in the next day or two.

  • worshiprocker

    I have a netbotz550 monitoring lab environments in our office building. I was wondering if it is possible to have the netbotz monitor shut down power to our APC switchable pdus if the temp gets to a set parameter? I am new to this system so please bare with me.

Page 1 of 1 (5 items)
Choose your language:  
powered by Communifire
Version 6.0.7119.9640