Loading ...

NetBotz 455 not picking up GSM Modem | Security & Environmental Monitoring Discussions

Home » Spaces » Security & Environmental Monitoring Discussions » discussion » General » NetBotz 455 not picking up GSM Modem

NetBotz 455 not picking up GSM Modem

Discussion in Security & Environmental Monitoring Discussions started by Artur , 1/28/2021 10:59 AM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

NetBotz 455 not picking up GSM Modem

Subscribe to RSS
  • Hello everyone, this is my first post here.

    I have a NetBotz 455 running on v4.7 that I wish to configure SMS alerts. However when I connect the GSM modem via the usb port, the NetBotz is not showing that a serial device has been connected via the usb port. I config reset the NetBotz, changed the firmware to lower versions but still the GSM is not being displayed on the NetBotz routerlogin. I have used the same type of GSM Modem on other NetBotz 455s and it works perfectly fine.

    Anyone with a solution to this problem?

    Thank.

     

     

  • Hello,

    NetBotz are actively supported at its own standalone community - https://help.ecostruxureit.com/questions

Page 1 of 1 (2 items)
Choose your language:  
powered by Communifire
Version 8.0.7757.16597