Hello,
i have bought a SmartUPS 6000 and have 6 MS Hyper-V 2016 Servers and 1 central Storage. Additional i have 1 extra machine on which is running the second AD DC (one is virtual). So i have 7 computers, 1 Storage and 1 UPS.My target is to shutdown all Hyper-V systems at once with all VMs on it, when power fails - at that point i do NOT want to migrate VMs automatically!If all Hyper-V systems are down, i want to shutdown the 7 th computer (with the AD on it) and after that the central Storage.
How can i do that?
Hi,
Please review the PowerChute Network Shutdown for Hyper-V User's Guide.
The guide will explain how to configure PowerChute with Hyper-V.
Choose a location
discussion :