we had yesterday only replaced our old APC RT 10000 UPS with a New SRC10KUXI UPS, our old UPS was working fine , but just for the sake of technology upgrade we purchased this new UPS.
But the new SRC10KUXI UPS is automatically switching to battery mode for a second and comes online and this happens very frequently, and some time in span of 4-5 minutes it happens 1-2 times...there is no power failure from our end all the connection are same which was for the old one, just we replaced the old UPS one with new UPS..
Overall configuration is
UPS: APC SRC10KUXI , BATTERY 65AH OF 32 NUMBERS
Same problem here, with multiple customers we expierence this.
I see the following logs:
4-10-19 10:32:10 Power Restored 4-10-19 10:32:09 Power Failed
And no loss of power.
Did u get any solution for the same, we request the team APC to reply on the same.
If the UPS is under warranty please register the call with toll-free, otherwise the check UPS firmware, if required update the firmware.
Choose a location
discussion :