Loading ...

Symmetra RM showing an "internal communication failure" | Getting Started

Home » Spaces » Getting Started » discussion » General » Symmetra RM showing an "internal communication failure"

Symmetra RM showing an "internal communication failure"

Discussion in Getting Started started by Roger , 3/13/2019 10:43 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Symmetra RM showing an "internal communication failure"

Subscribe to RSS
  • RogerinMD

    I recently had the batteries fail on this unit, showing a "internal temperature exceeded" which I found was due to a low center tap voltage in the sense circuit.  On restart of the unit, it will power up and report everything is operational until I turn on line power at which point it shows the internal communication failure with the RIM.  The unit will switch into bypass, but won't go online.

    Is there any additional checks or troubleshooting I can do?

    --UPDATE--

    The UPS will also come up with line power in maintenance bypass and everything plugged in but the battery.  All report OK in Diags until the battery goes in, then I get an internal communication failure and both Power Modules and the RIM report "NoCom-MIM/RIM".

    I might also add that in troubleshooting the original battery issue I pulled both the MIM and RIM at the same time, even though loads were off at the time.  I now read that this is bad.  Is there a reset procedure to get everything back in sync?

Page 1 of 1 (1 items)
Choose your language:  
powered by Communifire
Version 8.0.7598.8416