Loading ...

| Getting Started

Home » Spaces » Getting Started » discussion » General » Initial battery charge

Initial battery charge

Discussion in Getting Started started by Gene , 9/9/2016 7:02 PM
Login to follow, share, and participate in this space.
Not a member?Join now
Posted in: General

Initial battery charge

Subscribe to RSS
  • Geno

    What is the procedure for the initial charging of the battery on a SMC 1500? I’d assume it would be the same for all of them but that’s what I have. I find it hard to understand why there’s not one word on the subject in the manuals. Will it charge in the pwr off mode, does it require pwr on with the load unplugged or can the load be plugged in but be turned off and how long does it take?

  • voidstar

    Not sure how long it takes.

    Yes, as long as the UPS is plugged in, the charger will maintain the battery regardless of whether the UPS is "output on" or not. The load can but does not need to be attached.

  • GYJ1944

    I’m not clear if I should pull out something before I plug  the battery in. Step 2 is not clear to me. It shows opening pulling the battery out and then ? Should I do

  • GYJ1944
    On 1/21/2019 7:29 AM, Gloria said:

    I’m not clear if I should pull out something before I plug  the battery in. Step 2 is not clear to me. It shows opening pulling the battery out and then ? Should I do

    Please refer to connect the battery step 2

Page 1 of 1 (4 items)
Choose your language:  
powered by Communifire
Version 7.0.7496.13049