1 Reply Latest reply: Jan 5, 2012 7:27 AM by adrianmarsh RSS

"could not connect to the APC PowerChute Business Edition Server...."

adrianmarsh Member
Currently Being Moderated
Hi,

I'm trying to re-install Agent, Server and Console onto a single server, as the original passwords been lost.
Same version being used, same installation files.

I uninstalled the Agent, Server and Console and rebooted. I've then reinstalled the Agent and Server, running through their wizards setting the same username/password, and then finally installed the console. No issues running the wizards. I can access the Agents web interface with no problems.

When I try to login to the console though, using the same username/password, and an IP of 127.0.0.1, I get this 'could not connect to the apc powerchute business edition' error.

I've verified the Server service is running, and I've tried stop/starting it.
A netstat -anb shows that pbeser~1.exe is listening on TCP ports 2160 and 2260, and theres no firewall enabled on the server.

Any ideas ?

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 8 points
  • Helpful Answers - 4 points