4 Replies Latest reply: Jul 28, 2011 12:15 PM by Olin RSS

MGE UPS Pulsar EX 3200 RT Battery Falut Question.

mpeeng Member
Currently Being Moderated
This morning the UPS faulted and all the server rebooted, once the ups came back up I checked the properties page and I see that there is a battery fault and an alert (see attached picture). I click on the alert and I see this:

11      2011/07/25 07:56:35      Battery Fault
12      2011/07/25 07:56:37      No Battery
13      2011/07/25 07:56:37      Replace Battery
14      2011/07/25 07:56:37      Unavailable Battery

but on the properties page (see attached picture) under battery status it says the battery is fully charged and the last periodic test was ok.

What is the ups telling me? Do I need to replace the battery, or the whole system?

Thanks,

Jason

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 8 points
  • Helpful Answers - 4 points